Configure Users and Personnel Classes
Properties are used to define the unique attributes of your users and personnel classes.
Procedure
- In the navigator, click Personnel.
- In the Folders list, select the resource type you want to work with.Tip:As more lists appear, select the appropriate resource until you find the one you want to work with.
- In the Displays panel, click S95 Model Editor.
- Click the Properties tab, and then click Add Property.
- In the Name and Description fields, enter a name and description for the property/parameter.
- From the Data Type list, select a data type.
- In the Value field, enter a value for the selected data type.
- Optional: In the Unit of Measure field, enter a unit of measure for the selected data type.
- Click Save.