Workflow User Account Details

The Details tab on the S95 Model Editor for Workflow users offers general information about the selected user and allows you to create and configure the login credentials for your Workflow users.

You can change the name and description of this resource.

AttributeValueDescription
NameRequired; User-defined up to 50 charactersSpecifies a display name for a resource.
DescriptionUser-defined up to 255 charactersProvides more information about a resource that a user may find helpful.
AttributeValueDescription
Full NameUser-defined up to 255 charactersSpecifies the name of the user.
Note:
This name is for informational purposes in electronic signatures only. It is not a unique identifier and is not used for security credentials.
Create AccountN/AClick to create a new user account.
Remove AccountN/AClick to delete an existing user account.

User Account Status

The account status area indicates whether the selected Workflow user's account is active or disabled. A disabled account is an account that has been locked out due to exceeding the lockout threshold defined for your system. Only an Administrator user, or a user with the required permission can reactivate a locked out user account.

AttributeValueDescription
ActiveN/AIndicates that the current user account status is active.
Reactivate AccountN/AClick to reactivate a locked out Workflow user account.

Security Credentials

The following table describes the user-specific attributes on the S95 Model Editor required to configure the security credentials for a user. These attributes are available only when the Create Account button is clicked.

Note:
You can also access the security credentials for the selected user by clicking the Edit Security Credentials link on the Security Editor.
AttributeValueDescription
Login NameUser-defined alphanumeric string (A-Z, a-z, 0 - 9) up to 20 charactersSpecifies the unique login name for the selected user.
PasswordUser-defined alphanumeric string (A–Z, a–z, 0–9) up to 255 charactersSpecifies the unique password for the selected user.
Confirm PasswordUser-defined alphanumeric string (A–Z, a–z, 0–9) up to 255 charactersSpecifies the unique password for the selected user a second time.
E-mailUser-defined alphanumeric string (A–Z, a–z, 0–9) up to 255 charactersSpecifies the unique e-mail address for the selected user.