Configure Security Credentials for a User

About this task

Note:
You can edit a user's security credentials at a later time from either the S95 Model Editor or from the Security Editor.

Procedure

  1. In the navigator, click Personnel > People.
  2. In the People list, select the user you want to configure security credentials for.
  3. In the Displays panel, click S95 Model Editor.
  4. Click the Details tab.
  5. Optional: In the Full Name field, enter the user's name.
    This name is for informational purposes in electronic signatures only. It is not a unique identifier and is not used for security credentials.
  6. Click Create Account.
    The Credentials area expands, displaying further input fields
  7. In the Login Name field, enter a unique user name for the user you are configuring.
  8. In the Password field, enter the password for the user you are configuring.
  9. In the Confirm Password field, re-enter the password.
  10. Optional: In the Email field, enter the e-mail address of the user you are configuring.
  11. Click Save.
    This user is now active.