User and Personnel Class Properties
The Properties tab on the S95 Model Editor for Workflow users and personnel classes allows you to add, modify, and delete properties that are specific to a personnel class or person (user), or to view the properties for any personnel classes that are associated with the selected user.
The following table describes the information available on the Properties tab, where you can configure the values for the property attributes.
Attribute | Value | Description |
---|---|---|
List | User-defined | Displays a list of properties for the selected resource that can be arranged by name, type, and so on, depending on the property. These properties can be inherited from another resource or created for the current resource. |
Add Property | N/A | Click to add a new property. |
Delete Property | N/A | Click to remove the selected property. |
Name | User-defined alphanumeric string (A–Z, a–z, 0–9) up to 50 characters | Specifies a display name for the selected property. |
Description | User-defined alphanumeric string (A–Z, a–z, 0–9) up to 255 characters | Provides more information about a property that a user many find helpful. |
Data Type | System-defined | Specifies the data type of the property. Note:
|
Value | User-defined alphanumeric string (A–Z, a–z, 0–9) up to 255 characters | Specifies the value for the selected data type. Valid values depend on the selected data type. |
UoM (Unit of Measure) | User-defined alphanumeric string (A-Z, a-z, 0 - 9) up to 20 characters | Specifies the unit of measure for the data type, such as gallons, inches, tons. |