Configure security certificates for a click-once client

For a click-once client, use this procedure to install certificates using the certificate authority generated by the Workflow server installation.

About this task

Note:
Support for one-click installation of Workflow will be discontinued in a future release of the software. The client installation should be used when one-click installation is discontinued.

Procedure

  1. In the Workflow installation directory, go to the following folder to find the required certificate files: <installdir>\Program Files\Proficy\Proficy Workflow\Certificates\Export.
  2. Copy the following certificate files to your click-once computer:
    • ProficySelfSignedCA.pfx
    • ProficySTS.pfx
  3. For a click-once client running on Windows, run mmc.exe.
  4. From the Console window, go to the File menu, and then select Add/Remove Snap-in.
    The Add or Remove Snap-ins dialog box appears. In Available Snap-ins, double-click Certificates.
  5. In Available Snap-ins, double-click Certificates.
    The Certificates snap-in dialog box appears.
  6. Select Computer account, click Next, select Local computer, and then click Finish.
  7. Click OK.
  8. From Certificates (Local Computer), expand Trusted Root Certification Authorities\Certificates, and then add ProficySelfSignedCA.pfx.
  9. From Certificates (Local Computer), expand Personal\Certificates, and then add ProficySTS.pfx.