Configure quorum options for a cluster

Although this application does not require a disk for clustering, it is recommended that you configure either a file share witness or a disk witness.

Procedure

  1. On the server computer, click Start > Administrative Tools > Failover Cluster Manager.
    The Failover Cluster Manager dialog box appears.
  2. Select the cluster you want to configure.
    Tip:
    If the cluster you want to configure is not displayed, then in the console tree, right-click Failover Cluster Manager, click Manage a Cluster, and then select or specify the cluster you want to configure.
  3. From the Actions menu, click More Actions, and then click Configure Cluster Quorum Settings.
  4. Follow the instructions in the wizard to select the quorum configuration for your cluster.
    If you choose a configuration that includes a disk witness or file share witness, follow the instructions for specifying the witness.
  5. Optional: After the wizard completes and the Summary page appears, click View Report to view a report of the tasks that the wizard performed.