Clustering Tips

Use the clustering tips to ensure your failover cluster runs smoothly.

Security Certificates

When setting up a clustered environment, you must regenerate and export Proficy security certificates as part of configuring the primary cluster server, and then import the certificates when configuring the failover cluster server. Symptoms of incorrect security certificate configuration include the inability to create or display Silverlight forms and the Web Task List. For more information on setting up security certificates for a clustered environment, see Configure the Primary Server Cluster, Configure the Failover Cluster Server, and Modify Security Certificates.

Proficy Server Service is Marked for Deletion

Occasionally, after a server configuration, the Proficy Server service is marked for deletion. You can restore the service by running the Configure Server tool again.

Clients on Clustered Proficy Servers

Clients that are installed with clustered Proficy servers will work only if the server is the primary server.

Note:
If you have a cluster with multiple nodes, the cluster must be pointing to the client name, and the server that each node is running on must state the role name for the cluster. For more information, see Configure a local client for a cluster node (32-bit) and Configure a local client for a cluster node (64-bit).

Running a Clustered Multi-server Environment

When running with both a clustered application server and clustered Workflow/User servers, you must restart the primary server and then, after a few minutes, restart the primary Workflow/User server. This can be performed using the Microsoft Failover Cluster Manager by taking the servers offline, and then putting them back online.