Configure parameters in a test workflow

Before you begin

Note:
Parameters must have already been added to a workflow to configure them in a running workflow. For more information, see Add attributes to a workflow or subprocess.

Procedure

  1. In the navigator, click Workflow.
  2. In the Folders list, select a resource type, such as Workflows, Subprocesses, Schedules, User Activities, Categories, Completion Codes, Faults, or Filters.
  3. In the Displays panel, click Workflow Management > Workflow Editor.
  4. Click the Test/Debug tab.
  5. In a Set Workflow Input Parameters field, enter a value.
  6. To remove the value, click the arrow and select Reset to Default.