Test Parameters
You can configure the parameters of the workflow you are testing during the testing process.
The input parameters and test results sections display information only during a manual test of the current workflow. Test input and output parameters do not remain when you navigate from one workflow to another, and do not remain part of the workflow definition when the workflow is saved.
When you perform a test, you can reconfigure input parameters that are applied during this test only. When the test is complete, you can view the output parameters based on the results of the test. The values available for configuration are based on the parameters that have already been added in other configuration panels.