Configure a Status Message activity

Before you begin

Note: Activities can be inserted at both the workflow and subprocess levels.

Procedure

  1. In the navigator, click Workflow > Workflows.
  2. In the resource list, select the workflow that you want to work with. If no workflow exists, create a new workflow.
  3. In the Displays panel, click Workflow Management > Workflow Editor.
  4. Click the Workflow Editor tab.
  5. Insert an activity:
    • At the workflow level:
      • From the Standard Activities panel, click and drag the activity you want to insert to a drop point.
        Note: Activities can exist only between the presubprocess and postsubprocess.
    • At the subprocess level:
      • Double-click the local subprocess you want to add the activity to.
      • From the Standard Activities panel, click and drag the activity you want to insert to a drop point.
  6. On the activity configuration panel, select Update Status.
  7. In the Message field:
    • enter a message.
    • click the ellipsis button, and then in the Edit String dialog box, enter a message.
  8. If applicable, to include a bind or expression, click the drop-down arrow.
    Tip: For more information, see Property Value Types.
  9. Click Save.