Configure a message queue
This activity creates a message queue for sending or receiving messages between workflows or activities in order to coordinate work.
- Prerequisites
- Insert an activity
About this task
This activity creates a WorkflowQueue using the WorkflowQueuingService.
Procedure
- From a subprocess, drag and drop a Create Message Queue activity.
- In the Queue Name field, provide a name for the message queue. This value can be configured using a literal value, expression, or bind.Note:The following restrictions apply:
- The message queue name cannot be null or empty, and you cannot use workflow instance ID, task instance ID, or task step instance ID as a queue name, because doing so causes the activities to fault at run time.
- Empty GUIDs are not allowed.
- Leading and trailing spaces are trimmed in the queue name; otherwise, the queue name is invalid.
- If the queue name is not a reserved value but the queue already exists, no fault occurs.
- Click Save.