Send Message to Queue

This activity allows an author to configure a workflow to send a message to a queue by specifying the workflow instance ID, queue name, message type, and message in order to coordinate work between workflows and activities.

This activity interacts with a WorkflowQueue using the WorkflowQueuingService.
Note:
The following restrictions apply:
  • The message queue name cannot be null or empty, and you cannot use workflow instance ID, task instance ID, or task step instance ID as a queue name, because doing so causes the activities to fault at run time.
  • Empty GUIDs are not allowed.
  • Leading and trailing spaces are trimmed in the queue name; otherwise, the queue name is invalid.
  • A queue must be created before sending a message.
  • The workflow instance should be running before sending a message. If it is not running, the instance is not loaded/restarted.

Queue Configuration Properties

You are required to configure these properties for this activity.

PropertyValueDescription
Queue NameUser-defined; GUID; String

Specifies the name of the message queue, which is scoped to this workflow instance. This value can be configured using a literal value, expression, or bind.

Workflow Instance IDUser-definedSpecifies the unique identifier that is scoped to the queue name. The default value of the property must be bound to the Workflow.Instance ID property.

Message Input Properties

PropertyValueDescription
Message TypeUser-definedSpecifies the data type of the message being sent, which is scoped to this workflow instance.
MessageDepends on Message Type

Specifies the message being sent to another queue, which can be bound to the Receive Message from Queue activity. This value can be configured using a literal value, expression, or bind.