Configure a Form activity
Before you begin
A Form activity used in a workflow can either be configured to use a regular, hard-coded form, or it can be dynamic, where the form shown is determined at run time.
Procedure
- In the navigator, click .
- In the resource list, select the workflow that you want to work with. If no workflow exists, create a new workflow.
- In the Displays panel, click .
- Click the Workflow Editor tab.
- Drag and drop a Local Subprocess into the workflow and double-click it, or double-click an existing subprocess.
- To use the functionality of a form created in the Forms Designer, connect it to a Form activity by dragging and dropping it into the subprocess.
- In the Form field:
To use a... Do this... regular form - Click the ellipsis button to select your preconfigured form from the Universal Browser.
- Click OK.
dynamic form - From the drop-down arrow, select Bind to bind the form to a directory resource variable.
- In the Template field, click the ellipsis button to select a form template.
- Configure the available input parameters.
- Optional: Select the Allow user to cancel form check box.
- Optional: Select the Maintain form record upon completion check box if you want to view form data after a form has been completed.
- In the Out Comments field, configure the available output parameters.This field reflects the output available to the operator for the selected form.
- If applicable, to clear field contents, click the drop-down arrow, and then select Reset to Default.
- To activate the form at run time, click the Overview tab, and then click Enable.Note:Only activated subprocesses are available for workflows.
- Click Save.