Add an object to a dock panel

Procedure

  1. In the navigator, click Global Displays > Forms.
  2. From the Forms list, select the resource you want to work with.
  3. Click Display Editor > Designer.
  4. Click the Toolbox tab.
  5. Expand the control group you want to work with.
  6. Click and drag the control to the desired position in the Designer.
    Note:
    To apply the properties of a control to another control, click and drag the control to another control in the document tree. The Applying <control (control name)> to Target dialog box appears where you can select the option you want to use to apply to the control.
  7. Right-click the dock panel and select Edit Layer.
    The dock panel's editor is initiated, which is indicated by an orange border.
  8. From the Toolbox, click the object you want to add to the dock panel.
  9. Move the mouse pointer over the dock panel's editable area.
    The mouse cursor changes to a bold plus sign with the word "object."
  10. Click in the dock panel to add the object.
    Important:
    Objects cannot be explicitly positioned in a dock panel; therefore, objects cannot be drawn onto the dock panel and/or selected and moved.
  11. Configure the properties, as required.
    Note:
    To view the full list of properties, select the Advanced check box.
  12. Save the form or user display.
    Click Save on the...To save...
    toolbarlocally for WPF forms; to the server for Silverlight forms
    title barto the server for WPF forms