Configure control properties

Before you begin

Note:
Some properties are available only when a control is added as a child to another control. For example, the Dock property is available only when a control is added as a child to a Dock Panel control.

Procedure

  1. In the navigator, click Global Displays > Forms.
  2. From the Forms list, select the resource you want to work with.
  3. Click Display Editor > Designer.
  4. Click the Toolbox tab.
  5. Select the control you want to configure.
  6. Click the Properties tab.
  7. Configure the properties, as required.
    Note:
    To view the full list of properties, select the Advanced check box.
  8. Save the form or user display.
    Click Save on the...To save...
    toolbarlocally for WPF forms; to the server for Silverlight forms
    title barto the server for WPF forms