Media Controls

The media of a communications session is the form in which the data is transmitted. Media controls allow an application to recognize a variety of media types and adjust aspects of the media stream, such as the volume of voice transmission.

Media Controls Property Usage

The following table shows the properties used by each control:
PropertyMedia ControlVideo Text Block
AllowDropXX
BackgroundXX
BorderBrushXX
BorderThicknessXX
ClipToBoundsXX
ColumnXX
ColumnSpanXX
CornerRadiusX
EffectXX
FlowDirectionXX
FocusableXX
FocusVisualStyleXX
FontFamilyXX
FontSizeXX
FontStretchXX
FontStyleXX
FontWeightXX
ForceCursorXX
ForegroundXX
GlareBrush
HeightXX
HorizontalAlignmentXX
HorizontalContentAlignmentXX
IsEnabledXX
IsHitTestVisibleXX
IsManipulationEnabledXX
IsPlayingXX
IsSharedSizeScopeXX
IsTabStopXX
LocalizationXX
MarginXX
MaxHeightXX
MaxWidthXX
MinHeightXX
MinWidthXX
NameXX
OpacityXX
OpacityMaskXX
OverridesDefaultStyleXX
PaddingXX
PositionXX
RadiusXXX
RadiusYXX
RenderTransformOriginXX
RepeatX
RowXX
RowSpanXX
SnapsToDevicePixelsXX
SourceXX
StrokeThicknessXX
StyleXX
TabIndexXX
TagXX
TemplateXX
TextX
ToolTipXX
UidXX
UseLayoutRoundingXX
VerticalAlignmentXX
VerticalContentAlignmentXX
VisibilityXX
WidthXX

Media Controls Property Descriptions

The following table shows the properties descriptions used by all control:
PropertyDescription
AllowDropSelect this check box to indicate that the control can accept data that is dragged onto it.
BackgroundExpand this field to select the background color of the selected control.
BorderBrushExpand this field to select the border color of the selected control.
BorderThicknessSpecifies the border thickness of a control, in pixels.
ClipToBoundsSelect this check box to clip the content of this control (or content coming from the child elements of this control) to fit into the size of the containing control.
ColumnSpecifies the column within the grid where the control is located.
ColumnSpanSpecifies the total number of columns that child content spans within a grid.
CornerRadiusSpecifies the degree to which the corners of a control are rounded.
EffectClick the arrow to expand the property, select the effect you want to apply to the control, and then configure the specific values for the effect. Valid values to select are:
  • Blur
    • Kernel Type
    • Radius
  • Drop Shadow
    • Color
    • Direction
    • Opactiy
    • Shadow Depth
FlowDirectionSpecifies the direction that text and other user interface (UI) elements flow within any parent control. Selections are:
  • Left to Right
  • Right to Left
FocusableSelect this check box to indicate that the control can receive focus.
FocusVisualStyleSpecifies a property that enables customization of appearance, effects, or other style characteristics that apply to this control when it has focus.
FontFamilySpecifies the font family for the control.
FontSizeSpecifies the font size for the control.
FontStretchSpecifies the degree to which a font is condensed or expanded on the screen.
FontStyleSpecifies the font style for the control.
FontWeightSpecifies the weight or thickness of the specified font.
ForceCursorSelect this check box to indicate that the user interface (UI) renders the cursor as declared by the Cursor property.
ForegroundExpand this field to select the foreground color.
GlareBrushExpand this field to specify the glare effect for the control.
HeightSpecifies the height of the control, in pixels.
HorizontalAlignmentSpecifies the horizontal alignment characteristics applied to this control. Selections are:
  • Left
  • Center
  • Right
  • Stretch
HorizontalContentAlignmentSpecifies the horizontal alignment of the control's content. Selections are:
  • Left
  • Center
  • Right
  • Stretch
ImageStretchSpecifies how the image should be stretched to fill the destination rectangle. Selections are:
  • Fill
  • None
  • Uniform
  • UniformToFill
IsEnabledSelect this check box to indicate that this control is enabled in the user interface (UI).
IsHitTestVisibleSelect this check box to indicate that the control can possibly be returned as a hit test result from some portion of its rendered content.
IsManipulationEnabledSelect this check box to indicate that the manipulation events for the control are enabled.
IsPlayingSelect this check box to indicate that the control is playing.
IsSharedSizeScopeSelect this check box to indicate that controls are sharing size information.
IsTabStopSelect this check box to indicate that a control is included in tab navigation.
LocalizationClick the ellipsis button to open the Localization Configuration dialog box where you can configure the property to localize, the language to use for localization, and the text to localize.
MarginSpecifies the outer margin of a control.
MaxHeightSpecifies the maximum height of a control.
MaxWidthSpecifies the maximum width of a control.
MinHeightSpecifies the minimum height of a control.
MinWidthSpecifies the minimum width of a control.
NameSpecifies the identifying name of the control. The name provides a reference so that code behind, such as event handler code, can refer to a markup element during processing by a XAML processor.
OpacitySpecifies the opacity factor applied to the entire control. Valid values are 0 through 1, with up to 15 decimal places.
OpacityMaskExpand this field to select a color for the opacity mask, which is applied to any alpha-channel masking for the rendered content of this control.
OverridesDefaultStyleSelect this check box to indicate that this control incorporates style properties from theme styles.
PaddingSpecifies the amount of padding to apply to the inside edge of each side of a control.
PositionSpecifies the current position of progress through the media's playback time.
RadiusXSpecifies the x-axis radius of the ellipse that is used to round the corners of the rectangle.
RadiusYSpecifies the y-axis radius of the ellipse that is used to round the corners of the rectangle.
RenderTransformOriginSpecifies the center point of any possible render transform, relative to the bounds of the element.
  • X is the horizontal origin factor, given as a value between 0 and 1.
  • Y is the vertical origin factor, given as a value between 0 and 1.
RepeatSelect this check box to indicate that the video will repeat after the media has finished running through a continuous video cycle.
RowRowBackground
RowSpanSpecifies the total number of rows that child content spans within a grid.
SnapsToDevicePixelsSelect this check box to indicate that rendering for this control uses device-specific pixel settings.
SourceClick the ellipsis button to open the Navigate Uri dialog box to select the image source to use for the control.
  • Select the From Resource option to select an image source from the Resources directory in the Document Tree panel.
  • Select the From URI option to select the image source from a remote location.
StrokeThicknessSpecifies the width of the control's outline.
StyleSpecifies the style used by this control when it is rendered.
TabIndexSpecifies the order in which controls receive focus when the Tab key is pressed.
TagSpecifies an arbitrary object value that can be used to store custom information about this control.
TemplateClick the ellipsis button to open the Open dialog box to select a template to use.
TextSpecifies the text contents of a control.
ToolTipSpecifies the tool-tip that displays for this control in the user interface (UI).
UidSpecifies the unique identifier (for localization) for this control.
UseLayoutRoundingSpecifies a value that determines whether rendering for the object and its visual subtree should use rounding behavior that aligns rendering to whole pixels.
VerticalAlignmentSpecifies the vertical alignment characteristics applied to this control. Selections are:
  • Bottom
  • Center
  • Top
  • Stretch
VerticalContentAlignmentSpecifies the vertical alignment of the control's content. Selections are:
  • Bottom
  • Center
  • Top
  • Stretch
VisiblilitySpecifies the visibility of this control. Selections are:
  • Collapsed
  • Hidden
  • Visible
WidthSpecifies the width of the control, in pixels.