Motor and Fan Controls
Motors controls are graphical representations of motors, fans, and pumps, and rotary controls.
Motors provide a graphic illustration of how fast a motor is running by showing an indicator brush in the control. The speed of the motor is user-controlled; the faster the indicator moves, the faster the motor is running. By manipulating the properties, motor controls can be used to monitor motor behavior, lifespan, or even scheduled maintenance intervals.
Fan controls display the relative speed of rotation of the fan blades. Fans can be used as an independent control, or be added to a motor to simulate a motor fan.
When a motor or fan control receives a null value for the IsOn property, the control sets its Opacity property to 0.2. The control appears disabled until a True or False value is received for the IsOn property.
Rotary controls contain circular graphics that spin 360 degrees at user-defined rotation speeds. When a rotary control receives a null value for the IsOn property, the control sets its Opacity property to 0.2. The control appears disabled until a True or False value is received for the IsOn property.
Motor and Fan Controls Property Usage
Property | Centrifugal Pump | Gear | Heavy Motor | Helical Motor | Metal Fly Wheel | Multi Blade Fan | Paddle Wheel | Simple Fan | Small Fly Wheel | Sprocket | Square Motor | Tire | Wind Generator |
---|---|---|---|---|---|---|---|---|---|---|---|---|---|
AllowDrop | X | X | X | X | X | X | X | X | X | X | X | X | X |
Background | X | X | X | X | X | X | X | X | X | X | X | X | X |
BladeBrush | X | X | X | X | X | X | X | X | X | ||||
BladeStrokeThickness | X | ||||||||||||
BorderBrush | X | X | X | X | X | X | X | X | X | X | X | X | |
BorderThickness | X | X | X | X | X | X | X | X | X | X | X | X | |
CenterCapBrush | X | X | |||||||||||
ClipToBounds | X | X | X | X | X | X | X | X | X | X | X | X | X |
Column | X | X | X | X | X | X | X | X | X | X | X | X | |
ColumnSpan | X | X | X | X | X | X | X | X | X | X | X | X | |
Effect | X | X | X | X | X | X | X | X | X | X | X | X | X |
FlowDirection | X | X | X | X | X | X | X | X | X | X | X | X | X |
Focusable | X | X | X | X | X | X | X | X | X | X | X | X | X |
FocusVisualStyle | X | X | X | X | X | X | X | X | X | X | X | X | X |
FontFamily | X | X | X | X | X | X | X | X | X | X | X | X | |
FontSize | X | X | X | X | X | X | X | X | X | X | X | X | |
FontStretch | X | X | X | X | X | X | X | X | X | X | X | X | |
FontStyle | X | X | X | X | X | X | X | X | X | X | X | X | |
FontWeight | X | X | X | X | X | X | X | X | X | X | X | X | |
ForceCursor | X | X | X | X | X | X | X | X | X | X | X | X | X |
Foreground | X | X | X | X | X | X | X | X | X | X | X | X | |
GlareBrush | X | X | X | X | X | ||||||||
Height | X | X | X | X | X | X | X | X | X | X | X | X | X |
HorizontalAlignment | X | X | X | X | X | X | X | X | X | X | X | X | X |
HorizontalContentAlignment | X | X | X | X | X | X | X | X | X | X | X | X | |
IndicatorBrush | X | X | X | ||||||||||
InnerBorderBrush | X | X | X | X | X | X | X | X | X | ||||
IsEnabled | X | X | X | X | X | X | X | X | X | X | X | X | X |
IsHitTestVisible | X | X | X | X | X | X | X | X | X | X | X | X | X |
IsManipulationEnabled | X | X | X | X | X | X | X | X | X | X | X | X | X |
IsOn | X | X | X | X | X | X | X | X | X | X | X | X | |
IsSharedSizeScope | X | X | X | X | X | X | X | X | X | X | X | X | |
IsTabStop | X | X | X | X | X | X | X | X | X | X | X | X | |
Localization | X | X | X | X | X | X | X | X | X | X | X | X | X |
Margin | X | X | X | X | X | X | X | X | X | X | X | X | X |
MaxHeight | X | X | X | X | X | X | X | X | X | X | X | X | X |
MaxWidth | X | X | X | X | X | X | X | X | X | X | X | X | X |
MinHeight | X | X | X | X | X | X | X | X | X | X | X | X | X |
MinorBackground | X | X | X | X | X | X | X | X | X | X | X | X | |
MinWidth | X | X | X | X | X | X | X | X | X | X | X | X | X |
MotorSpeed | X | X | X | X | X | X | X | X | X | X | X | ||
Name | X | X | X | X | X | X | X | X | X | X | X | X | X |
Opacity | X | X | X | X | X | X | X | X | X | X | X | X | X |
OpacityMask | X | X | X | X | X | X | X | X | X | X | X | X | X |
OverridesDefaultStyle | X | X | X | X | X | X | X | X | X | X | X | X | X |
Padding | X | X | X | X | X | X | X | X | X | X | X | X | |
RenderTransformOrigin | X | X | X | X | X | X | X | X | X | X | X | X | X |
RotationSpeed | X | X | X | X | |||||||||
Row | X | X | X | X | X | X | X | X | X | X | X | X | |
RowSpan | X | X | X | X | X | X | X | X | X | X | X | X | |
ShowGridLines | X | ||||||||||||
SnapsToDevicePixels | X | X | X | X | X | X | X | X | X | X | X | X | X |
StrokeThickness | X | X | X | X | X | X | X | X | X | ||||
Style | X | X | X | X | X | X | X | X | X | X | X | X | X |
TabIndex | X | X | X | X | X | X | X | X | X | X | X | X | |
Tag | X | X | X | X | X | X | X | X | X | X | X | X | X |
Template | X | X | X | X | X | X | X | X | X | X | X | X | |
TertiaryBackground | X | X | |||||||||||
TertiaryBorderBrush | X | X | X | ||||||||||
TertiaryStrokeThickness | X | X | |||||||||||
ToolTip | X | X | X | X | X | X | X | X | X | X | X | X | X |
Uid | X | X | X | X | X | X | X | X | X | X | X | X | X |
UseLayoutRounding | X | X | X | X | X | X | X | X | X | X | X | X | X |
VerticalAlignment | X | X | X | X | X | X | X | X | X | X | X | X | X |
VerticalContentAlignment | X | X | X | X | X | X | X | X | X | X | X | X | |
Visibility | X | X | X | X | X | X | X | X | X | X | X | X | X |
Width | X | X | X | X | X | X | X | X | X | X | X | X | X |
Motor and Fan Controls Property Descriptions
Property | Description |
---|---|
AllowDrop | Select this check box to indicate that the control can accept data that is dragged onto it. |
Background | Expand this field to select the background color of the selected control. |
BladeBrush | Expand this field to select the color of the blade. |
BladeStrokeThickness | Specifies the thickness of the blade. |
BorderBrush | Expand this field to select the border color of the selected control. |
BorderThickness | Specifies the border thickness of a control, in pixels. |
CenterCapBrush | Expand this field to select a color for the center cap. |
ClipToBounds | Select this check box to clip the content of this control (or content coming from the child elements of this control) to fit into the size of the containing control. |
Column | Specifies the column within the grid where the control is located. |
ColumnSpan | Specifies the total number of columns that child content spans within a grid. |
Effect | Click the arrow to expand the property, select the effect you want to apply to the control, and then configure the specific values for the effect. Valid values to select are:
|
FlowDirection | Specifies the direction that text and other user interface (UI) elements flow within any parent control. Selections are:
|
Focusable | Select this check box to indicate that the control can receive focus. |
FocusVisualStyle | Specifies a property that enables customization of appearance, effects, or other style characteristics that apply to this control when it has focus. |
FontFamily | Specifies the font family for the control. |
FontSize | Specifies the font size for the control. |
FontStretch | Specifies the degree to which a font is condensed or expanded on the screen. |
FontStyle | Specifies the font style for the control. |
FontWeight | Specifies the weight or thickness of the specified font. |
ForceCursor | Select this check box to indicate that the user interface (UI) renders the cursor as declared by the Cursor property. |
Foreground | Expand this field to select the foreground color. |
GlareBrush | Expand this field to specify the glare effect for the control. |
Height | Specifies the height of the control, in pixels. |
HorizontalAlignment | Specifies the horizontal alignment characteristics applied to this control. Selections are:
|
HorizontalContentAlignment | Specifies the horizontal alignment of the control's content. Selections are:
|
ImageStretch | Specifies how the image should be stretched to fill the destination rectangle. Selections are:
|
IndicatorBrush | Expand this field to select the color to use for the graphical indicator (pulse) of the motor speed. |
InnerBorderBrush | Expand this field to select the color for the inner border. |
IsEnabled | Select this check box to indicate that this control is enabled in the user interface (UI). |
IsHitTestVisible | Select this check box to indicate that the control can possibly be returned as a hit test result from some portion of its rendered content. |
IsManipulationEnabled | Select this check box to indicate that the manipulation events for the control are enabled. |
IsOn | Select this check box to indicate that the control is turned on. |
IsSharedSizeScope | Select this check box to indicate that controls are sharing size information. |
IsTabStop | Select this check box to indicate that a control is included in tab navigation. |
Localization | Click the ellipsis button to open the Localization Configuration dialog box where you can configure the property to localize, the language to use for localization, and the text to localize. |
Margin | Specifies the outer margin of a control. |
MaxHeight | Specifies the maximum height of a control. |
MaxWidth | Specifies the maximum width of a control. |
MinHeight | Specifies the minimum height of a control. |
MinorBackground | Expand this field to select the fill color of secondary components on the control. |
MinWidth | Specifies the minimum width of a control. |
MotorSpeed | Specifies the relative motor speed of the control. |
Name | Specifies the identifying name of the control. The name provides a reference so that code behind, such as event handler code, can refer to a markup element during processing by a XAML processor. |
Opacity | Specifies the opacity factor applied to the entire control. Valid values are 0 through 1, with up to 15 decimal places. |
OpacityMask | Expand this field to select a color for the opacity mask, which is applied to any alpha-channel masking for the rendered content of this control. |
OverridesDefaultStyle | Select this check box to indicate that this control incorporates style properties from theme styles. |
Padding | Specifies the amount of padding to apply to the inside edge of each side of a control. |
RenderTransformOrigin | Specifies the center point of any possible render transform, relative to the bounds of the element.
|
RotationSpeed | Specifies the rotation speed of the control. |
Row | RowBackground |
RowSpan | Specifies the total number of rows that child content spans within a grid. |
ShowGridLines | Select this check box to indicate that grid lines are visible within this grid. |
SnapsToDevicePixels | Select this check box to indicate that rendering for this control uses device-specific pixel settings. |
StrokeThickness | Specifies the width of the control's outline. |
Style | Specifies the style used by this control when it is rendered. |
TabIndex | Specifies the order in which controls receive focus when the Tab key is pressed. |
Tag | Specifies an arbitrary object value that can be used to store custom information about this control. |
Template | Click the ellipsis button to open the Open dialog box to select a template to use. |
TertiaryBackground | Expand this field to select the inner background color. |
TertiaryBorderBrush | Expand this field to select the innermost border color of the selected control. |
TertiaryStrokeThickness | Specifies the width of the control's innermost outline. |
ToolTip | Specifies the tool-tip that displays for this control in the user interface (UI). |
Uid | Specifies the unique identifier (for localization) for this control. |
UseLayoutRounding | Specifies a value that determines whether rendering for the object and its visual subtree should use rounding behavior that aligns rendering to whole pixels. |
VerticalAlignment | Specifies the vertical alignment characteristics applied to this control. Selections are:
|
VerticalContentAlignment | Specifies the vertical alignment of the control's content. Selections are:
|
Visiblility | Specifies the visibility of this control. Selections are:
|
Width | Specifies the width of the control, in pixels. |