Slider
The Slider control enables you to select a value from a range of values, usually from a minimum to a maximum, along a continuum. For example, the volume on a stereo. The left-hand side usually represents minimum value and the right-hand side usually represents high (the maximum) value, with a range of values in between.
The Slider control has a horizontal or vertical orientation, a track, and a movable thumb. A slider’s track can be annotated to show starting and ending points and ticks for the different values along the continuum. Unlike a scroll bar, a slider’s thumb remains fixed – both in size and in relation to the value it represents.
Common properties used on the slider are Minimum, Maximum, Value, and Orientation.
See Common Controls to view the usage and description of the properties for this control.