Polyline
The Polyline control is used to create drawings, graphic designs, and user interfaces. A polyline draws linear (that is, straight) lines by connecting a number of specified points. Whereas a simple line control contains only one line between two end points, a polyline can contain an infinite number of points.
Unlike a rectangle or an ellipse, a polyline is drawn as an unfinished shape, meaning that the starting and ending points of a polyline are left open and unconnected. But, similar to other finished shapes, a polyline is capable of displaying a fill color or design on the inside of the connected lines and end points.
See Shape Controls to view the usage and description of the properties for this control.