Dual Gauge
A Dual Gauge control is a radial gauge with a circular shape. The dual gauge has the ability to display two different variables from within the same display face.
The gauge contains two needles, two sets of ticks and two tick rings. The default value for the control is the Value property, and operators may also want to find to the InnerValue property.
The Batch Generic Button control causes multiple events to occur each time the button is pressed.
See Gauge Controls to view the usage and description of the properties for this control.