Compile Errors

Compile errors occur when there is a problem with a workflow and it cannot execute.

Workflow Errors

When a workflow resource is invalid, such as a subprocess or user activity, you receive an error message that you can view in the Overview section of the Workflow Editor, or in the Feedback Zone. The type of errors you see can be either configuration errors, such as a broken binding, or external errors, such as a missing resource being referenced in the workflow (for example, a data item). You can use the compile feature to resolve an issue with external resources only. For example, if you restore a missing piece of equipment, you can use the Compile button to make the workflow valid.

The following table describes the available options.

AttributeValueDescription
View ErrorsN/AClick to view errors related to the current workflow.
CompileN/AClick to recompile a workflow after you resolve the error.