When you install Standard Plant Applications Web Client, both Process and Discrete services and applications are installed by default. However, post-installation, you can disable the Discrete applications. Disabling the Discrete applications is a two step process:
Disable the services from the web server
Hide the applications from the Operations Hub server
Disable the services from the web server
Procedure
Extract the enable-disable-discrete-utility-master.zip file located at the <Installation_Directory>\GE Digital\PlantApplicationsWebClient directory.
After the zip file is extracted, open the enable-disable-discrete-utility-master folder.
In the enable-disable-discrete-utility-master folder, run (run as administrator) DisableDiscrete.bat.
A command prompt appears for you to enter the tomcat installation location.
At the Enter Tomcat Installation path prompt, enter the path where tomcat is installed in double-quotes. For example, "<tomcat_home>/Apache Software Foundation/Tomcat 9.0".
You will be prompted to enter the Web Client installation path.
At the Enter Web Client Installation path prompt, enter the path where Web Client is installed in double-quotes. For example, "C:\Program Files\GE Digital\PlantApplicationsWebClient\OperationsHub_PostingUtility".
All the Discrete applications will be disabled. A DiscreteBackUp folder is created under the <Installation_Directory>\GE Digital\PlantApplicationsWebClient path and all the Discrete services files are moved to this folder. This in turn is used in future if you want to enable the Discrete applications.
Hide the apps from Operations Hub
Procedure
Access Ophub designer with Ophub tenant user credentials :
https://<ophub-host>/iqp
Select Plant Applications under Apps.
Select NAVIGATION located the top-left corner of the screen.
You need to delete the following Discrete Apps:
Unit Operations
Work Order Manager
Route Editor
WorkQueue
Time Booking
Select the app and then select the Delete icon.
Repeat the same for all discrete applications.
Now, when you access the Web Client, the Discrete applications are not visible in the left panel.