Standard Edition Web Client Requirements

Before you begin

Ensure that you have completed following tasks :
Review the following preinstallation requirements before you run the Plant Applications Web Client installer:

System Requirements

Ensure that your computer meets the system requirements as described in the following table. For more information, refer to the System Requirements section in the Plant Applications Getting Started Guide document for the latest Plant Applications release.

Item Version
Operating system 64-bit Windows 10, Windows Server 2012 R2, Windows Server 2016, or Windows Server 2019
Couch DB server CouchDB version 2.3.1 and later installed and configured on a Windows machine. GE also supports CouchDB 3.2.2.
Note: For more information on configuring CouchDB, refer to Configuring Apache CouchDB Settings.
Web browsers Chrome 85.0 or later , with minimum resolution 1366x768.
Devices:
  • iPad: Safari v13.1+, Chrome 85.0 or later with resolution 2048x1536
  • HP tablet: Chrome 85.0 or later , with minimum resolution 1920x1280
    Note: Devices supports only Unit Operations,Work Queue, and Non Conformance applications.
    .
OLEDB Driver Microsoft OLE DB Driver 18 for SQL Server
Note: You can download the Microsoft OLE DB Driver 18 for SQL Server from the following URL: https://www.microsoft.com/en-us/download/details.aspx?id=56730.
Hard drive 100 GB (minimum)
Processor 2.4 GHz clock-speed Intel Core i3, i5, or i7 CPU or equivalent AMD Phenom CPU
Note: For better performance, it is recommended to use a octa core (8-cores) processor.
Memory 32 GB (recommended)
Note: You must have 64 GB or more if you plan to install Web Client (Both Process and Discrete), Historian, Operations Hub, and Plant Applications on the same node. However, it is recommended to install them in a distributed environment.

Port Requirements

Ensure that the ports described in the following table are opened before you install Plant Applications Web Client.
Port Description
15672 The default port for the RabbitMQ Message bridge required to communicate with the Plant Applications server for retrieving data updates.
8090/8091 The default port for the Tomcat server.
1433 The default port for the Microsoft SQL server.
9093 The default port for Kafka.
2185 The default port for ZooKeeper.
6984 The default port for CouchDB.
5059 The default port for Web Applications