Installation Overview

Plant Applications Web Client contains two types of applications:
  • Process: Contains the applications that are used in a process or continuous manufacturing model (for example, bottle or paper manufacturing).
  • Discrete: Contains the applications that are used in a discrete manufacturing model (for example, motor or bike manufacturing).
The following methods of installation are available:
  • Standard Installation: This is used to install Plant Applications Web Client for both Process and Discrete applications on a Windows machine. You can choose this method of installation if you want to perform a first-time installation to upgrade from a previous version of Plant Applications Web Client.
  • Enterprise Installation: This is used to install Plant Applications Web Client for both Process and Discrete applications on a Linux machine. You can choose this method only for a first-time installation of Plant Applications.

To troubleshoot any issues during the installation or upgrade process, refer to the Troubleshooting section in this guide.