About Installing Standard Web Client
Installing Plant Applications Standard Web Client installs both the process and discrete applications. You must perform this type of installation if you want to upgrade from a previous version of Plant Applications. You can choose this method for a first-time installation as well.
The following table outlines the steps that you must complete to install Plant Applications Standard Web Client for the first time. These tasks may be completed by multiple people in your organization. We recommend, however, that the tasks be completed in the order in which they are listed. All steps are required unless otherwise noted.
Step | Task | Notes |
---|---|---|
1 | Install Operations Hub 2.0 | This step is required. |
2 | Configure CouchDB for HTTPS | This step is required. |
3 | Ensure that your system meets the requirements for the Standard Web Client installation. | This step is required. |
4 | Install Standard Web Client | This step is required. |
5 | After the Standard Web Client installation, ensure to run the Message Bridge Configuration utility. | This step is required. |
6 | After configuring Message Bridge, ensure to run the Operations Hub Posting utility. | This step is required. |
7 | Verify the Installation | This step is required. |