Post Plant Applications Web Client Configuration to Operations Hub
Procedure
- After performing Step-2, from the main menu, select 3 to post the Plant Applications Web Client installation configuration parameters (which are the result of updating Docker Swarm to Plant Applications 8.1) to Operations Hub.
- Enter values for each prompt as specified in the following table.
Prompt Description Enter Operations Hub server name Enter the host name or the IP address of the Operations Hub server. Enter Operations Hub Tenant User Enter the UAA tenant username of Operations Hub. Enter UAA Admin ClientID Enter the UAA admin client ID. Enter UAA Admin Client Secret Enter the UAA admin client secret. A folder named OperationsHub_Post is created in the installation folder. If the failed count is 0, the installation is successful. - Enter 4 to exit the installer.
- Copy the OperationsHub_Post folder to a folder in the Operations Hub (Windows) server.
- Access the folder in the Operations Hub server, and run the InstallWebComponents.cmd file as an administrator.The Web Client plug-ins are placed in the Operations Hub server.