The Docker Web Client’s installer has default configuration selections that are optimized for Linux machines of 32 GB RAM. With the default installation, the maximum number of concurrent clients / scalability will be limited to 10 or 12. If your scalability requirements are high and need to support over 100 concurrent client sessions, you must choose the target Linux server with 64-GB RAM. Also, before starting the installer you must perform following task.
For some reasons, if you have performed the installation with the default settings, that is, without making any changes to the plantapps-web-docker.j2 file as stated above and realized that the default installation is not supporting your scalibillity requirements , you can make the following changes to repair the installation to meet your scalability requirements to utilize RAM size of 64 GB.