Installation Overview
Plant Applications Web Client contains two types of applications:
- Process: Contains the applications that are used in a process or continuous manufacturing model (for example, bottle or paper manufacturing).
- Discrete: Contains the applications that are used in a discrete manufacturing model (for example, motor or bike manufacturing).
The following methods of installation are available:
- Without using a Docker container: This is used to install Plant Applications Web Client for either Process, Discrete, or both applications. You can choose this method of installation if you want to perform a first-time installation to upgrade from a previous version of Plant Applications Web Client.
- Using a Docker container: This is used to install Plant Applications Web Client for both process and discrete applications. You can choose this method only for a first-time installation of Plant Applications.
To troubleshoot any issues during the installation or upgrade process, refer to the Troubleshooting section in this guide.