Modify a Process Order Status
Procedure
- Log in to Plant Applications Web Client.
- Select . By default, the Open page appears, displaying a list of process orders grouped by the associated execution path in a tabular format. You can select the Closed tab if you want to change the status of process orders that are in the completed status.
- From the Actions column, select for a required process order.Based on the current status of the process order, you can perform any of the following actions:
- If the current Status is Pending, then you can either select Next or Planning based on the valid transition states configured for the execution path to which the process order belong.
- If the current Status Next, then you can select Active or Pending based on the valid transition states configured for the execution path to which the process order belong.Note: Activating a process order makes it the current running process order that product quantities, process order run times, and process order statistics are applied to.
- If the current Status Active, then you can select Complete or Pending based on the valid transition states configured for the execution path to which the process order belong.Note: For a given execution path, you can have only one process order that is in active or next state. Completing an Active process order allows a different process order to be activated. If another process order has a status of Next, it will automatically become the Active process order when the current Active process order is moved to Complete.
- Optional: Alternatively, you can change the status of a process order from the Process Order Details page.In the Process Order Details page, select and then select the required status from the available options.