About the Work Queue Application
As an operator, you can use the Work Queue application for maintaining a list of operations that you must perform, and report the status of completion of each operation.
Each row in Work Queue represents an operation to be performed. By default, Work Queue contains the operations in which at least one serial number is currently clocked on by you. You can add additional operations that are ready or in progress to Work Queue.
Using the Work Queue module, you can perform the following tasks:
- Access an operation.
- Add operations to Work Queue.
- Clock on a serial or lot.
- Clock off a serial or lot.
- Provide data for a quality variable.
- View the status of an operation.
- Access documents associated with an operation.
- Access a list of BOM parts associated with a serial or lot.
- Specify the consumption of BOM parts during production.
- Specify whether you have completed working on a serial or lot.
- Creating a non-conformance.
- Add a comment.