About Adding a Comment
While working on a serial/lot, you can add a comment on the serial/lot or the work order to provide any additional information.
You can view the comment added to a serial/lot regardless of the operation you are performing on the serial/lot. For example, if you have added a comment to a serial/lot while performing the first operation, the comment also appears when you access the serial/lot for any subsequent operations. Similarly, when you add a comment to a work order, it appears when you access any of the serials/lots for the work order. For this reason, when you add a comment, it is a good practice to provide the details of the operation for which the comment is applicable.
If a work order or serial/lot contains comments, when you access an operation, the comments button () appears with a blue dot (). If you select that button, the number of comments for the work order or serial/lot appears on the Work Order or Serial/lot tabs, respectively.
- Microsoft Word (DOC/DOCX)
- Microsoft Power Point Presentation (PPT/PPTX)
- Microsoft Excel (XLS/XLSX)
- text document