Overview
Plant Applications Web Client acts as a container of the applications for managing work orders as described in the following table.
Application | Description |
---|---|
Unit Operations | Displays a list of operations associated with a work order. You can track the progress of completion of an operation, access reference documents, provide data for quality variables, specify consumption of BOM items, and create a defect. |
Non Conformance | Displays a list of nonconformities raised as defects on serial numbers or material lots. The application includes details for each defect and enables you to select a disposition plan for each defect or access a record of the disposition plan taken on each defect. |
Work Order Manager | Displays the status, progress, and priority of work orders. You can also modify a work order and its plan, access the work order, history, defects, and manage the planned dates of a work order, if required. |
Route Editor | Displays the routes used to manufacture a product. You can create routes, add operations to the route, assign BOM items, equipment, documents, and properties to the operations, and release a route for use in a work order. |
Work Queue | Displays a list of operations that are ready or in progress. You can add operations to the queue, track the progress of completion of an operation, access reference documents, provide data for quality variables, specify consumption of BOM items, and create a defect. You can clock on, complete, record completed quantity, and/or raise defects on multiple serials/lots at the same time. |
Time Booking | Enables an operator or supervisor to view labor records (timesheet), add missing time records, and modify the applied time of a previously submitted record. |
Property Definition | Displays a list of property definitions tailored to the requirements of your business. The application also displays the property groups and categories to which a property definition belongs. |
Security | Displays a list of applications to which the logged-in user has access. |
Configuration | Enables a system integrator to perform the following tasks in the Unit Operations and Work Queue applications:
|
Approval Cockpit | Enables an administrator to configure, execute, and track approval workflows for action events. |
Downtime | Displays the list of KPIs and downtime events for the machines assigned to the operator. |
OEE Dashboard | Displays an overview of the OEE, Quality, Performance, and Availability KPIs. Additional information about each KPI is displayed as Pareto and Waterfall charts. |
Reports | Displays KPI reports and production status of the plant by department, line, and unit. It also provides information about Planned vs. Actuals for each KPI. |
My Machines | Enables an operator to subscribe and monitor the required machines for downtime events. |
Analysis | Plots historical and live charts to visualize time series data available in Plant Applications and Historian. Displays information for production batches in the form of a Gantt chart. |
OEE Aggregation Store | Calculates and stores OEE data in a database so that it is quickly accessible. The OEE data can be calculated at the site level. The OEE data can be refreshed at a configured interval. |
Activities | Displays the activities planned within the duration of a shift. You can add an activity for an event within the shift duration, and then any user can perform the activity within the shift duration. |
Process Orders | Monitors the progress of the process orders. Active process orders track actual production and quantities against process orders, and display remaining quantities, planned quantities, planned start times, and planned end times. |
Alarms | Triggers alarm notifications based on rules configured in Plant Applications Administrator. |
Waste | Enables an operator or supervisor to create records for a waste event and associate it with a production event. |