About the Time Booking Application
As an operator or supervisor, you can view your labor records (timesheet). You can also add missing time records, or modify the applied time of a previously submitted record. When an operator performs a clock off, the time difference between the clock on and clock off is the default calculated applied labor time for that labor record. In the event of any discrepancy, you can manually adjust the applied labor time.
You can use the Time Booking application in the following scenarios:
- an operator has made a mistake related to vouchering a transaction (for example, clocked off 10 minutes late)
- an operator forgot to clock off at the end of a shift
- an operator did not clock on at all for the day
- the vouchering or punchout system was not working
- the MES system was down
Users with an operator role have access to view and edit records that were transacted by them. Users with a supervisor role can view and edit records for other users, in addition to managing their own records.
Important: A submitted labor record cannot be deleted, regardless of the role of the submitter.
Operators and supervisors can adjust the applied labor time for three types of operation statuses:
- ready
- in-progress
- completed
Operators and supervisors can perform the following tasks in the Time Booking application:
- View the labor records by a time period.
- Create a labor record. The following labor types are available:
- Direct
- Rework
- Setup
- Indirect
- Modify the applied time for a labor record.