Modify a Process Order
Procedure
- Log in to Plant Applications Web Client.
- Select . By default, the Open page appears, displaying a list of process orders grouped by the associated execution path in a tabular format. You can select the Closed tab if you want to edit process orders that are in the completed status.
- From the Actions column, select for a required process order.
- From the menu, select Edit.The Edit Process Order page appears.
- As needed, modify process order parameters as required in the General and Advanced sections.Note: When you associate a bill of materials formulation with a process order, only the formulations associated with the selected product will be available for selection.
- Optional: In the General section, select Add Comments to either add, modify, or delete comments for the process order.The Add Comment window appears.
- In the ADD COMMENT box, enter a comment for the changes you made, and select Add.Note: You can modify or delete only those comments that were added by you. However, based on the site parameter, you can also update comments from other users if you have the required permissions.
- Select Save.Note: The changes made to the process order are saved.