Dispose Multiple Defects
- Create a PlanNote: A plan can only be created in NC view.
- Enter the plan number in the search bar. The plan is added to the queue in the Home page.
- Select the plan number from the queue. All the defects associated with the plan appear on the Home page
- Select
.
The Disposition page appears. The disposition page displays the number of defects being disposed. - In the???Select Disposition???drop-down list, select an option as described the following table.
Option
Description
Clear
Select???Clear???if the defects raised for the non-conforming parts are not considered as defects.
Continue to process
Select???Continue to process???to allow operation on the non-conforming parts and then select the operation till which you can continue the operations process, in the???Select operation???drop-down list box.
Use as is
Select???Use as is to use the non-conforming parts in the operations as they are.
Scrap
Select???Scrap???to discard the non-conforming parts.
Rework
Select???Rework???to rework on the non-conforming parts and then select the operation on which the parts should be reworked, in the???Select operation???drop-down list box.
The???Select reasons???window appears. - In the???Select reasons???window, select a corrective disposition action reason and the associated sub reasons, as applicable. Tip: In the???Search???box, enter a disposition action reason to search for, and then select the reason from the reasons list.
- Optional:???In the???ADDITIONAL INFORMATION???box, enter any relevant information such as a URL, contact details of the supplier, or any information that is helpful to perform the root cause analysis of the non-conformance.
- Select???Submit.