Clock Off a Serial/Lot for an Operation
Before you begin
Procedure
- In the Work Queue page, in the row containing the operation on which you want to stop working, select OFF.Note: The OFF button is enabled only if you have clocked on at least one serial/lot in the operation.The Select Serial number(s) to clock off window appears, displaying a list of serials/lots in the operation that you have clocked on.
- If you want to clock off all the available serials/lots, select the check box in the heading column of the table.
- If you want to clock off selected serials/lots, perform one of the following steps:
- Select the check box for each serial/lot that you want to clock off.
- Search for a serial/lot by entering the value in the Search in available serial numbers box, and then select the check boxes from the filtered list that appears.
- Scan the bar code of the serial/lot by selecting
.
Note: By default, during Plant Application installation,LotsToExecute
is set to 50, so you can only clock off 50 serials/lots at a time. If you want to change the value, you must edit theLotsToExecute
property and set a new numerical value.If you have installed Enterprise Plant Applications Web Client, this parameter is available in the following file:
After you change the value of the parameter, run the following Docker commands to restart the Work Queue application:<installation_path>/PlantApplicationsDocker/plantapps-web-docker/mnt/configfiles/workqueue-app/prod/<version>/workqueue-app-prod.properties
-
sudo docker service scale PAContainer_workqueue-app=0
-
sudo docker service scale PAContainer_workqueue-app=1
If you have installed Standard Plant Applications Web Client, this parameter is available in the following file:
After you change the values of parameters, restart the Work Queue application.C:\Program Files\GE Digital\PlantApplicationsWebClient\config-repo\workqueue-app\prod\<version>\workqueue-app-prod.properties
- Select Clock off.
Results
- The selected serials/lots are clocked off. In the Work Queue page, the number of serials/lots that are clocked on is updated in the OFF/ON column.
- When you clock off all the serials/lots of a work order that previously had all the serials/lots clocked-on, the labor type of the work order displayed in the header is changed to the default value.
Important: The Clock on/off button will not appear, if
you modify the BEHAVIOR of an operation to Non Clocking
in the Attributes tab of a route in the Route Editor application.