If you want to add operations by scanning the bar code of a serial number, ensure that the camera has been enabled.
Procedure
In the Work Queue page, in the Enter a serial/lot no. or work order or operation to add to queue box, enter the name of the operation or work order that you want to add to Work Queue. You can also enter a serial number on which you want to perform an operation.
Select .
Tip: You can also scan the bar code of the serial number by selecting .
Results
If you entered (or scanned) a serial number, the operations that you can perform on the serial number are added to Work Queue.
If you entered the name of an operation, all the operations that contain the name and are ready are added to Work Queue.
If you entered the name of a work order, all the operations in the work order are added to Work Queue.