STATUS | The status of the operation. |
OP | The name of the operation. |
WORK ORDER | The unique identifier of a work order. |
DESCRIPTION | The description of the operation. |
SERIAL/LOT | If the work order contains only one serial/lot, this column contains the unique ID of the serial/lot. If the work order contains multiple serials/lots, this column contains a link, specifying the number of serials/lots in the work order. When you select the link, a window appears, displaying the statuses and IDs of all the serials/lots in the work order for the operation. Note: The value in this column does not include the number of serials/lots that are in the Cancelled status. |
COMPLETED | The number of serials/lots for which the operation has been completed out of the [total number of serials/lots minus planned quantity of skipped serials/lots] on which you must perform the operation. |
SCRAP | The number of serials/lots that have been scrapped during the operation. |
ON HOLD | The number of serials/lots that are on hold. |
SKIP |
The number of serials/lots that are skipped. |
EXCLUDED QTY |
The number of operations excluded in a mutually exclusive
set. |
ON/OFF | Contains buttons to clock on or clock off an operation. The number in the ON button indicates the number of serials/lots that are clocked on. These buttons are disabled for an operation that does not require clocking on. |
OPT |
Indicates that the operation is
Optional by displaying OPT against
the operation. |
COMP/REC | Contains the following buttons: : Allows you to provide the completed quantity for an operation on a serial/lot. : Allows you to mark an operation complete after the completed quantity for a serial/lot equals the planned quantity.
: Allows you to skip an operation that in Ready status. For more information, refer
|
COMPLETED | Indicates whether the operation is complete. |