Save an Analysis Trend
About this task
Procedure
- Log in to the Plant Applications Web Client.
- Select
.
The Chart Configuration page appears.
Note: For every new session, when you login and selectfor the first time, the default trend chart appears. You can close the chart to go back to the Chart Configuration page.
- Select a plant model and data type for which you want to view the trend chart.
- Depending on the data type, select Add Chart or Add Batches, and then select Plot.
-
Select
.
The Save Trend window appears.Each field that appears in the Save Trend window is described in the following table.
Field Description Title Enter a descriptive name for the chart. Saved Charts Displays the folder tree view under Saved Charts for you to save a trend. You can either select an existing folder or you can create a new folder using the icon. You can perform below actions by selecting a required folder.
Note: Theicon indicates that the current default trend is saved in this folder.
Actions The actions that you can perform for saving a trend. You can select one of the following action items: : Select to add a new folder.
: Select to mark a trend as default. This appears only when you select an existing trend from a folder. For more information, refer Mark a Saved Trend as Default.
Note:indicates that the selected trend is the current default trend.
: Select to rename a folder or a trend name.
: Select to delete a saved trend. For more information, refer Delete a Saved Trend.
: Select to go a level above the current folder. Alternatively, you can use the breadcrumbs to navigate through the current directory.
: Select to refresh the list of files and folders for a selected folder.
-
Select Save Chart.
The current analysis view is saved as an analysis trend and is accessible by all users.Tip: To restore or delete the saved trend, select
in the Chart Configuration page. For more information, refer to the Restore a Saved Trend and Delete a Saved Trend topics.