NAME | Identifies the name of the route. Enter a unique value that does not exceed 100 characters. |
DESCRIPTION | Identifies the description for the route. Enter a value that does not exceed 1000 characters. |
BOM FORMULATION | Identifies the BOM formulation that you want to use in the route. This box contains a list of BOM formulations configured for the material in Plant Applications Administrator. You can select a value. |
BEHAVIORS |
Use the check boxes to enable the following behaviors for
the route:
- Require Work Order to be completed
manually - This behavior allows for
support of work orders to be completed manually by a
supervisor. The default behavior is to not support
manual completion, but to auto-complete the work
order when all lots are completed.
- Allow addition of material lots to a work
order in progress - This behavior
allows operators or supervisors to add lots to a
work order while it is in progress, regardless of
the planned quantity for the order. This behavior
can be set only on routes that are for serialized
products.
|