In the Route Editor application, click an existing route name to modify it
(if you need to create a new route, see Add a
Route). This will bring up the Edit ROUTE page.
Click the Resources tab.
Group by Operation or Equipment.
Click the chevron for the operation you are going to modify.
Optionally you can select a value for each of Machine Labor Codes and
People Labor Codes. If you specify a code for either of these labor types,
you must enter a Standard Time. You have the option of entering a Standard
Time without selecting a labor code.
Enter a Standard Time for the each of the four labor planning types for each
of Machine and People. Times entered must be in the format
hh:mm:ss.