Access List of Operations
About this task
Procedure
Access a Route for which you want to view the operations.
The list of operations in the route appears, displaying the Overview section. The following table provides information on each column in the table.
Column | Description |
---|---|
SEQ | The sequence number of the operation. |
NAME | The name of the operation. |
DESCRIPTION | The description of the operation. |
BEHAVIOR | The behavior of the operation. The following options are available:
|
LABOR TYPES | The labor type of the operation. |
DEFAULT LABOR | The default labor type. |
EQUIPMENT | The equipment that is used to perform the operation. There can be multiple equipment for the same operation. |
MUTUAL EXCLUSION | Switch the toggle to make the operation as mutually
exclusive to another operation. Note: You can make an
operation mutually exclusive to another operation that
has the same sequence number (priority). |