This procedure is usually performed
when a new material is added to Plant Applications. A system administrator or a super
user at the site can perform this procedure. When a part is created in Plant
Applications (either directly or through an external interface), you must perform a
basic set up to use Receiving Inspection.
Procedure
If the UOM of the material that you want to add does not exist in Plant
Applications, perform the following steps:
Tip: To check if the UoM of the material exists, select Global Configuration > Engineering Units > Units.
Create an engineering record for every unit of measurement (UOM)
associated with the material lots that you want to inspect.
Create a new production event sub-type named Received Material
Lot-<UOM> for every UOM that you have created. Configure these new
event sub-types to use the appropriate UOM.
Create a product family with a name appropriate for your business
(e.g., Receiving and Inspection).
Create a product property named Receiving and Inspection, and configure
it to create the characteristics on the Receiving and Inspection product
family.
Create a characteristic for every material that you want to inspect
using the Receiving and Inspection product property.
A product for the characteristic will be created.
Make sure that every inspected material under the Receiving and
Inspection family has the default characteristic for the Receiving and
Inspection product property set to a characteristic that matches the
product code.
If this is a first-time set up, create the following specification
variables under the Receiving and Inspection product property:
Auto Complete (logical)
TCR-Critical Criteria (string)
TCR-Part-specific Criteria (string)
TCR-Common Criteria (string)
%Serial Numbers to test (For Serialized)
%Samples to test (Integer) (For Non-Serialized)
Enter the target specifications for all characteristics for the
specification variables that you have created.
Create a characteristic for every material that you want to inspect
using the Receiving and Inspection product property.
A product for the characteristic will be created.
Make sure that every inspected material under the Receiving and
Inspection family has the default characteristic for the Receiving and
Inspection product property set to a characteristic that matches the
product code.
Enter the target specifications for all characteristics for the
specification variables that you have created.
If the material that you want to add has UOM and a corresponding unit:
Create a characteristic for every material that you want to inspect
using the Receiving and Inspection product property.
A product for the characteristic will be created.
Make sure that every inspected material under the Receiving and
Inspection family has the default characteristic for the Receiving and
Inspection product property set to a characteristic that matches the
product code.
Enter the target specifications for all characteristics for the
specification variables that you have created.