Access the receiver for which you want to generate samples. You can generate samples only for a material lot for which inspection tests are defined in Plant Applications Administrator (indicated by ).
Procedure
In the left pane, under the receiver, select the material for which you want to generate samples.
The Edit Traceability section appears.
If you do not want to split the lot:
Enter a number in the LOT NUMBERS column.
Enter the quantity in the QTY column.
If you want to generate samples for a periodic inspection, under the
Periodic Inspection column, ensure to select
the check box and enter the quantity.
Note: Once you select a part and its quantity for periodic inspection,
you cannot change the quantity or the inspection type for that
lot.
If you want to split the lot:
In the LOT NUMBERS column, select .
A new row appears for the sublot. Repeat this step depending on
the number of sublots you want to create.
For each sublot, enter a value in the LOT NUMBERS
column. This value must be unique for the lot.
For each sublot, enter the quantity in the QTY column.
If you want to generate samples for a periodic inspection, under the
Periodic Inspection column, ensure to select
the check box and enter the quantity.
Note: Once you select a part and its quantity for periodic inspection,
you cannot change the quantity or the inspection type for that
lot.
As needed, enter values in the remaining fields.
Select Save.
Changes to the lot are saved.
Note: You can continue to change the lots
until the inspection begins. After you enter the inspection criteria, you
cannot change the lots.
Select Generate Samples.
The Generate Samples button is enabled only if the sum
of the quantities of all the sublots is equal to the total number of items in
the lot.
Samples are generated for the lot or each sublot and appear in the
Inspection Criteria section. The size of the sample is
calculated based on the size of the lot or sublot. The status of the receiver
changes to awaiting inspection (indicated by ).