Install the Plant Applications Client and Administrator
About this task
The client installation installs the Plant Applications Client and Administrator, Plant Applications Excel Add-in, Downtime Supervisor Screens, and Help files. It also installs Development tools and remote services, including the Plant Applications OPC Server and Remote Data Services. Plant Applications Administrator is the primary means of maintaining and managing the Plant Applications software. You can control system security by limiting the number of computers with the Administrator program installed.
To make it easier for technical support to quickly correct any potential problems, install the Plant Applications Administrator and Client software on the same computer as the Plant Applications Server. Also, install the Administrator and Client software on workstations that maintain the Plant Applications configuration.
Procedure
- Select Plant Applications Client from the Installation Menu, then select Next on the Welcome screen.
- When prompted, select OK to review the Important Product Information page.
-
From the Custom Setup page, select Plant
Applications Client and Plant Applications Excel
Add-in from the list of options.
You can also select Plant Applications Administrator, OPC Server, and Remote Data Services to install.
No prerequisite software is required to install the Proficy OPC Server. However, you can use an OPC test client such as Matrikon OPC Explorer to test connections to the OPC Server. See Plant Applications Help to set up a user account.
Select Space to display the available and required space for features.
-
Select Next to continue.
You are prompted to install Microsoft Excel, if needed.
- Enter the name of the SQL database server or select Browse button to select one. Select Next to continue.
-
On the next page, accept or change the destination folder.
You are prompted to install desktop shortcuts. Select Yes if you want to install desktop shortcuts.
- Select Yes to allow Plant Applications to bypass firewall and port settings, or to make appropriate setup changes.
-
From the Ready to Install page, select
Install.
The Installing Plant Applications Client screen is displayed as the wizard installs the software and completes post-installation tasks.
- When the wizard displays the InstallShield Wizard Completed page, select Finish. Ignore an error message related to a file unzip action not responding.