Plant Applications Server and Client Requirements
Before you install Plant Applications, verify that all required software versions have been installed on the target machine.
Workflow is required for Plant Applications and can be installed from the Installation Menu.
See Test and Production Environments to compare machine requirements in a test, standard production, and high-transaction environment.
The Plant Applications Server and Web Client servers can be hosted in the AWS/Azure Cloud. Ensure that when they are hosted in Cloud, they meet the Plant Application and Web Client Server system requirements.
Operating System
- Microsoft® Windows® Server 2022 (64-bit) for server installations
- Microsoft® Windows® Server 2019 (64-bit) for server installations
- Microsoft® Windows® 10 (64-bit) for Client installations
Network Interface Software
- Internet Protocol Version 4 (IPv4)
Microsoft®.NET Framework
- Microsoft .NET Framework 4.7 for Workflow 2.6 SP1Note: You can download the Microsoft .NET Framework 4.7 from the following URL: https://go.microsoft.com/fwlink/?LinkId=825299
- Microsoft .NET Framework 4.7.2 for Plant Applications Server
- Microsoft .NET Framework 3.5 for Plant Applications Client
- Microsoft .NET Framework 4.7.2 or later for Plant Applications Report Server (Migrated)
Microsoft® SQL Server®
- Microsoft® SQL Server® 2019 (with the latest
Cumulative Update installed), 2017 (64-bit), and 2016 (64-bit)Note: You must have SQL Server 2016 (64-bit) and later for the Plant Applications Server and Web Client installation. If you are running a previous version of SQL Server, a message stating that the prerequisite criteria not met appears. You must upgrade to SQL Server 2016 (64-bit) and later to continue with the installation.
- Microsoft System CLR Types SQL Server 2016 (32-bit only)Note: Do not install if you already have the Microsoft System CLR Types SQL Server 2016 (32-bit only) installed.
- SQL Server 2012 Native Client version 11.4.7001.0 or laterNote: The SQL Server 2012 Native Client is required for Plant Applications Server, Plant Applications Web Server, and Plant Applications Client machines. If the version of the SQL Server 2012 Native Client you installed is the version before 11.4.7001.0, you must upgrade it. You can download the SQL Server 2012 Native Client version 11.4.7001.0 or later from the following URL: https://www.microsoft.com/en-us/download/details.aspx?id=50402
- For information on SQL Server requirements, refer to SQL Server Requirements.
Software Requirements
Software | Requirement |
---|---|
Web Server | IIS 8.0 or later based on the operating system |
Microsoft Office | Microsoft Excel 2021, 2019, or 2016 (required for SQL Server and
Web Engines) 32-bit. Note: If you import data using a Microsoft Excel
file that was created in an older version, it will not contain
the columns necessary to support the new Event Progress feature.
Refer to topics in Plant Applications Help for steps describing
how to use the Excel add-in. |
Document Viewer | PDF reader (required to view some Web Server reports) |
Workflow | Workflow 2.6 SP1 Note: You must install Workflow 2.6 SP1 if you are installing a clean environment of Plant Applications. |
Browsers |
Note: Process Analyzer only supports Chrome.
|
Communication | MAPI-compliant Mail client software |
Server Hardware Requirements
Minimum Requirement | GE Recommended |
---|---|
The minimum server requirements when running a Plant Applications environment without SOA entities and not using the Client or Workflow:
|
For a standard implementation, GE recommends the following:
|
Client Hardware Requirements
- Pentium 4-based computer with 2 GB of RAM (minimum)
- 20-GB hard drive space (minimum)
- DVD drive
- Network interface software for network communications supporting TCP/IP
- Monitor for the lab and floor operations, 100 percent IBM compatible, supporting a 24-bit graphics card for 1024 x 768 or higher resolution and at least 65535 colors
- Two-button mouse with scroll wheel or compatible pointing device such as a touch screen
Supported Small Screen Devices
- iPad 6th Gen: Safari v13.1+, Chrome 107.0.5304.107 and laterNote: To view the application content, you must select the desktop site option from the Chrome browser settings menu.
- HP tablet: Chrome 107.0.5304.107 and later
- Android 10-inch Tablet: Chrome 107.0.5304.107 and later.Note: To view the application content, you must select the desktop site option from the Chrome browser settings menu.
- Activities
- Downtime
- OEE Dashboard
- Reports
- My Machines
- Alarms
- Process Orders
- Waste
- Unit Operations
- Work Queue
- NCM
Port Requirements
Use internal interfaces to open the ports required for Plant Applications operations.
Port | Description |
---|---|
80 | Used by Web server for serving traditional web reports. |
1433 | Used by SQL Server for communication to SQL. |
Use the CXS_Service
table in the Plant Applications database to modify the following ports.
Port | Description |
---|---|
12293 | Used by Proficy Server Manager for the Service Control feature of the Administrator. |
12294 | Used by Proficy Server Gateway for clients (including SDK) to send/receive Plant Applications messages. |
12295 | Used by Proficy Server Gateway for clients (including SDK) to send/receive Plant Applications messages. |
12295 | Used by older (4.0 and older) versions of Client Manager. |
12299 | Used by Proficy Server Remote Data Service, allowing Proficy services perform remote read and write operations to a historian. |
12401 | Used by Proficy License Manager for licensing requests from Proficy services to clients. |
5762 | Used by Plant Applications Web Client to connect to RabbitMQ. |
Use INI files such as cmRTR.ini, cmConfigMgr.ini, PlantAppsMessging.ini, or Message.ini (found in the Plant Applications program installation directories), to modify the following ports:
Port | Description |
---|---|
10000 | Used by the Proficy message router to process Plant Applications messages between services clients communicating with the router. |
12280 | Used by the Proficy message router to process Plant Applications messages between services clients communicating with the router. |
Language Support
Plant Applications supports the following languages for translation:
Languages | Plant Applications Client | Plant Applications Web Client | |
---|---|---|---|
Process Available in versions above |
Discrete Available in versions above |
||
US English | YES | 8.0 | 8.0 |
Arabic | YES | 8.0 | 8.1 |
Bosnian | YES | 8.2 | |
Chinese (Simplified) | YES | 8.0 | 8.1 |
Czech | YES | 8.1 | 8.1 |
Danish | YES | 8.0 | |
Dutch | YES | 8.0 | 2022 |
Finnish | YES | 8.0 | |
French (European) | YES | 8.0 | 2022 |
German | YES | 8.0 | 8.2 |
Hebrew | YES | 8.0 | |
Italian | YES | 8.0 | 2022 |
Japanese | YES | 8.0 | 8.1 |
Korean | YES | 8.0 | |
Russian | YES | 8.0 | 8.2 |
Polish | YES | 8.0 | |
Portuguese (Brazilian) | YES | 8.0 | 2022 |
Slovenian | YES | 8.0 | |
Spanish (Latin American) | YES | 8.0 | 8.2 |
Swedish | YES | 8.0 | |
Turkish | YES | 8.0 | 8.2 |
Vietnamese | YES | 8.1 | 8.1 |
Compatibility with Other GE Products
GE Software | Supported Version |
---|---|
Operations Hub | 2.1 with SIM3 and later, 2022, 2023 |
Workflow | 2.6 SP1 |
Historian | 7.0 SP6, 8.1, 9.1, 10.0, 2022, and 2023 |
iFIX | 6.1, 6.5, 6.8, 2022, and 2023 |
CIMPLICITY | 11.0 SIM2 and 2022 |
For silent installers, see Silent Installers