Mark an Operation Complete
Before you begin
-
If you do not have the permission to perform this task, request your administrator to provide the permission using Security.
- For a non-serialized product, if the operation that you want to mark complete requires clocking on, provide the completed quantity for the operation.
About this task
After all the operations on all the serials/lots in a work order are marked complete, the work order is marked complete in Plant Applications. You can view the completion status of the work order in Work Order Manager.
For example, Lot A is set for an initial planned quantity of 10. Now, at operation-1, the operator claims 9 of 10 quantity and completes the operation. In the Work Queue application, the operation-1 is complete with 9 of 10. However, for the next operation (operation-2), Lot A produces 10 quantity based on the initial planned quantity (and not as previous manufactured/created/recorded quantity of 9 at operation-1). In the Work Order Manager application, the work order can be completed with 9 of 10.
Procedure
- Select the operation that you want to mark complete.
- In the left pane, select the serial/lot for which you want to mark the operation complete, and then select
.
Note: Thebutton appears only if the completed quantity of the serial/lot equals the planned quantity for the work order or if the operation does not require clocking on.
Tip: You can search for a serial/lot by entering a value in the search box or by scanning for the bar code using theicon, and then selecting the check boxes from the filtered list that appears.
For a lot with thresholds, the RECORD QUANTITY window appears. - Select Rec + Complete.You do not have to enter a quantity.