Access a List of Operations
About this task
As a supervisor, you can access operations in the Ready, In Progress, On Hold, and Completed statuses associated with a production line or material family.
Procedure
- In the Work Order Manager page, select one of the following tabs:
- Released: Select this tab if you want to access a list of operations that are ready or in progress.
- On hold: Select this tab if you want to access a list of operations that are on hold.
- Completed: Select this tab if you want to access a list of operations that are completed.
- Select By Operations.A list of operations in the status that you have selected appears. The following table provides information on the columns in the table.
Column Description STATUS The status of the operation. OPERATION The name of the operation. SERIAL/LOT The serial/lot number on which the operation is being performed. WORK ORDER The work order for which the operation is performed on serials/lots. MATERIAL FAMILY The material family associated with the material. MATERIAL The name of the material associated with the work order. COMP QTY The quantity of serials/lots completed or produced out of the total quantity of serials/lots on which the operation must be performed. The value in this column appears in the following format: <completed quantity> of <planned quantity> (for example, 2 of 5). PRI The priority of the work order. For instructions on how to prioritize a work order, refer to the Prioritize a Work Order topic. UNIT The production unit on which the operation is performed. STARTED ON The date and time when the operation has begun. The date and time appear in the following format: mm/dd hh:mm (for example, 03/27 10:58). For an operation in the Ready status, the value in this column is blank. READY ON The date and time when the operation was ready. The date and time appear in the following format: mm/dd hh:mm. OPT Indicates that the operation is Optional by displaying OPT against the operation.