A conditional electronic signature can be used to override
the defined electronic signature settings when certain other conditions (variable
definitions) you configure are met.
Procedure
Configure the stored procedure
dbo.spActivities_GetCustomEsignatureLevelForVariables (which
ships with Plant Applications). You will need access to the Plant Applications
database as well as administration/database owner permissions to modify this stored
procedure.
Note: When modifying this procedure, be sure to maintain its input and output
structures.
Ensure the variable plant.apps.override-variable-esignatureLevel
(located in the activities-app-service-prod.properties file) is
set to true (the default is false).
Depending on your installation,
activities-app-service-prod.properties will be located
at: