ORDER |
The recommended order of consumption of the BOM item in an operation. |
MATERIAL |
The material number of the BOM item. |
MATERIAL DESC |
The material description of the BOM item. |
REQ QTY |
The planned quantity of the BOM items required for the completion of the serial/lot for the operation. |
CONSUMED QTY |
The actual quantity of the BOM items consumed during the production. |
UOM |
The unit of measure (UOM) of the BOM item. |
SERIAL/LOT# |
The serial/lot of the raw material that was consumed. |
LOWER QTY |
The lower tolerance quantity of the BOM item that can be consumed. |
UPPER QTY |
The upper tolerance quantity of the BOM item that can be consumed. |
SCRAP FACTOR |
The Percentage of this BOM item that is expected to be lost during production of the formulation. For example, if 100 units of Product XYZ is required with a scrap factor of 1%, then you should have a 101 units on hand when preparing to produce the product. |
STORAGE UNIT |
Unit currently storing the selected product. |
SUBSTITUTIONS |
The replacement materials available for that item as a
substitution. |